11/10/2017 4:41 PM | |
Posts: 37 Rating:
|
I guess it is because node-red can not longer access its standard in/out/error file handles and it it receives the "HUP" signal (hangup) when you close the terminal.. To avoid this, you would redirect stdout, stderr and stdin to /dev/null:
There is a tool called "nohup" which can be used to suppress this, but it's probably not installed on the IoT:
Michael
|
Last edited by: turner42 at: 11/10/2017 4:47:32 PMLast edited by: turner42 at: 11/10/2017 4:50:02 PM |
|
This contribution was helpful to
2 thankful Users |
11/10/2017 7:45 PM | |
Joined: 4/28/2015 Last visit: 6/28/2024 Posts: 578 Rating:
|
nohup is installed, in fact, but starting via the run script that iot2000setup creates is the recommended way. |
Follow us on