11/15/2017 8:08 PM | |
Joined: 1/12/2015 Last visit: 1/1/2024 Posts: 2 Rating:
|
I am tearing my hair out with this!!!! "Please Help" I have completed the following tasks with Azure IoT
So I feel I have everything at the latest version to make it work but all I get is either one of these debug faults in node red. using the mqtt protocol I get the debug message "Could not connect: certificate is not yet valid" and no increase in messages on the Azure IoT hub I have checked the ssl status and have the berkeley cert in the appropriate directory although when checking the ssl status I get error code 20... using the amqp protocol I get the debug message "Error while trying to send message:NotConnectedError: AMQP Transport: Could not connect" and no increase in messages on the Azure IoT hub I have tried a combination of shared keys across the AzureIoT node and the injection function using a JSON string in case I need the device id one in one place and the IoT hub in another but this makes no difference... Every now and again I get a List Keys operation in the Activity log but its random to me... At the moment my view is that the IoT2040 is not the correct device for looking at a solution that connects devices to the cloud which is disappointing as I'd like a complete Siemens solution in an industrial environment I hope the forum can help change my mind!!!!! PS I have following davide_maffei guide to no avail including changing the azure-iot contrib node. this makes no difference.... PPS my npm list at depth 0 is as follows :- +-- azure-iot-device-amqp@1.2.2 +-- mraa@1.5.1 +-- node-red@0.17.5 +-- node-red-contrib-azureiothubnode@0.1.21 +-- node-red-dashboard@2.1.0 +-- node-red-node-intel-gpio@0.0.5 +-- node-red-node-serialport@0.4.1 `-- npm@3.10.9 ------------------------------------------------------------------------------------------ |
Last edited by: Lee_G at: 11/15/2017 8:11:01 PMLast edited by: Lee_G at: 11/15/2017 8:14:32 PMLast edited by: Jen_Moderator at: 11/16/2017 11:45:48 AMNew subject after splitting |
|
Follow us on