5/29/2017 8:45 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating:
|
Hi, just an idea. We had the same problems with node-red-contrib-opcua in the past. The problem was the node version on the IOT2000. The OPC UA node requires node version >6 as I remember and on our last image V2.1.2 we had the version 4.x.x. Maybe this could be the same problem with our version 6.9.2 now. I am trying to find out if there are any dependencies like that. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
11/15/2017 5:22 PM | |
Posts: 439 Rating:
|
Hello bergmanu, Sorry for the delay. So, I update Node-RED with PuTTY using:
I can now see it up to date to v0.17.5. I retried the installation and got the same errors. So I thought maybe it was related to NPM, so I also updated it. I used:
I retried:
and now I get: It seems to be related to GIT, so I search about this issue and found the below Google group exchange of a guy with the same issue as mine. BACnet interface to Node RED - Google Groups
Oh oh... How to Install Git on IOT2040?
Am I stuck? Would it be possible for me to manually take the files on GitHub and put them in IOT with WinSCP?
Best regards, Hugo |
11/16/2017 4:47 PM | |
Posts: 439 Rating:
|
Hello, Not use to let go easily... I move the file from the GitHub project into node folder via WinSCP. I tried many commands to install the node... https://github.com/goliatone/node-red-contrib-bacnet
https://groups.google.com/forum/#!topic/node-red/fNce4rT613M
Then: The result are always the same. As I put the JSON, HTML and other files into a node folder called "bacnet", I tried running the below command from that folder:
The result changed at this point: It seems the JSON file contains java which is the reason why it can't be parsed... (I'm lost at this point) If I look at the log here is what I can see:
Does anyone have a tips? Best regards, Hugo |
Last edited by: HugoD at: 11/16/2017 4:48:30 PM |
|
11/24/2017 12:19 PM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating:
|
New question published by eric00058 is split to a separate thread with the subject Node-red-dashboard: widget cannot identify the input. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on