11/28/2017 4:07 PM | |
Joined: 5/17/2010 Last visit: 5/22/2024 Posts: 226 Rating:
|
Hi, at HWConfig you find the I/O address range of the DP-Slave at the slot overview when the focus is on DP-slave object. This address range can be directly used at your PLC program for data access. You can use these input bits directly at your PLC programming like you do this with local I/O modules. Same for output addresses of SIMOCODE-DP. .E.g. Output Bit x.2 is used for start command. All the mentioned bit assignment are default settings but it is also possible to change this assignment at SIMOCODE-DP parameterization. That's why you need to check how the assignment is parameterized to make sure you use the correct bits at PLC programming. Further detailed information on SIMOCODE-DP: Manual SIMOCODE-DP Motor Protection and Control Device: With best regards Michael |
------------------------------------------------------------------------------------------------ |
|
Follow us on