11/28/2017 5:24 PM | |
Joined: 8/2/2007 Last visit: 8/22/2023 Posts: 4 Rating: (0) |
Hello, I am trying to set up Python on the IOT 2040 and am following a guide found here. The problem I’m running into is that nothing seems to be able to install from the Python repository. I have included an example of the error below. I was wondering if there is a python setup that is more recent. "Collecting pytz Could not fetch URLhttps://pypi.python.org/simple/pytz/: There was a problem confirming the ssl certificate: [SSL: CERTIFICATE_VERIFY_FAILED] certificate verify failed (_ssl.c:645) - skipping Could not find a version that satisfies the requirement pytz (from versions: ) No matching distribution found for pytz" Thanks, rags Can anyone guide me |
Last edited by: rags at: 12/4/2017 2:37:15 PM |
|
This contribution was helpful to1 thankful Users |
12/4/2017 5:48 PM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (379)
|
Hi, the following error may be caused by the date&time of your IOT. If this isn't the current time there may be some issues regarding the SSL certificates.
You can set the time with the command
I tried to install the package pytz and it worked.
Please note that the link you are referring to is 1 year old. Pretty sure that there is another version of the example image used. So if you are using the latetst example image V2.1.3 just type in pip3 install pytz. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on