1/13/2018 3:11 AM | |
Joined: 6/12/2017 Last visit: 3/3/2024 Posts: 5 Rating: (0) |
Hi It's my first project with tia v14 and my plc s7 1518-4 PN/DP. Also have a 2 Gb memory card. There is a lot of memory space but when I try to download software (simulation or plc). Error "There is not enough memory space on the CPU for this amount of data" occurs I have reviewed Configuring Messages and Alarms in WinCC (TIA Portal) and found "The number of configurable alarm blocks depends on the SIMATIC controller used. More detailed information can be found in the corresponding SIMATIC controller system manual." But I could not find the number of maximum program alarm. Maybe there is another reason for it, I am not sure... There are my screenshots from memory usage and error. Do you have any suggestions ? Thanks.
|
1/13/2018 10:15 AM | |
Posts: 8946 Rating: (999) |
Please give us a picture of the MMC that you have insert into the CPU... |
This contribution was helpful to1 thankful Users |
1/13/2018 11:56 AM | |
Joined: 6/12/2017 Last visit: 3/3/2024 Posts: 5 Rating: (0) |
I have these... |
Follow us on