1/4/2018 3:37 PM | |
Posts: 3 Rating: (2) |
Is it possible to rename already existing and used CMT? I am using PCS7 V9.0 and I have a case when a CMT called MS01 shall be renamed to SBE_MS01. CMT Name in Techn.I/Os is assigned to chart (via Add chart). I rename the CMT in the master data library (MDL) (MS_01 -> SBE_MS01). Then I open the PH folder in the AS and the CMs indicate that they belong to the right CMT (renamed - SBE_MS01). So far ok. When I run Synchronisation it indicates that Assigned name of CMs is different (A: empty, B: SBE_MS01). On a lower level (chart) I get also indication of difference (A: MS_01, B:SBE_MS01). When I run the synchronization, the first CM in PH folder in AS is renamed from e.g. EE-77-0061A to SBE_MS01 and all other attempts for renaming the others fails (of course). Is it possible to rename CMTs once the CMs exists? And how to do it correctly? What happens if the change in the MDL is done while one of the AS Projects is removed/checked out from the MultiProject?
AttachmentCMT_Renaming_Screenshots.zip (62 Downloads) |
Last edited by: Petr_S at: 1/9/2018 10:54:34 AM |
|
Follow us on