1/8/2018 4:20 AM | |
Posts: 72 Rating: (0) |
Hi experts, Do you know if PWM can be simulated via PLC Sim V14. After configuring the device (CPU 1511C-1PN) and active the PWM function, and give the control interface (12bytes) all necessaries value, and i got the feedback 0000_0000 in feedback interface (4 bytes). So i think i fail to simulate PWM function. Can some one give me some advice ? Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/17/2018 1:37:32 PMNew subject after splitting |
|
1/17/2018 5:43 PM | |
Joined: 7/7/2010 Last visit: 6/4/2024 Posts: 14766 Rating: (2377)
|
I believe if you look in the plc sim documention (F1-Help), it clarifies the limitations of the simulator. From what I saw in a quick scan for the s7-1500 family, PWM functionality is supported. My advice is to make sure you enable the PWM, and that you use the control block to configure the PWM at run-time.
|
science guy |
|
Follow us on