2/10/2015 3:30 PM | |
Joined: 4/24/2006 Last visit: 6/17/2024 Posts: 8683 Rating: (1159) |
Hello Rodrigo, Have a look at the following link: Updates for STEP 7 V13 and WinCC V13 You only need to install update 6.
There is even already Service Pack 1 for TIA Portal V13: Service Pack 1 for STEP 7 V13 TIA Portal
Best regards, Wizard
|
2/10/2015 4:18 PM | |
Posts: 5225 Rating: (1189) |
Dear Wizard - I am having doubts on recommending fellow users to upgrade to TIA13 SP1 when I read so many are having issues with the upgrade. Our office is holding back too. Do you have an opinion to share on this? In our case, I am wondering also if it is better to remove TIA13 Update 6 and then do a clean install of TIA13 SP1. The steps I would suggest: .... but then before starting it would be a good idea to backup ("clone") your computer. Any thoughts on this matter?
|
Last edited by: William B. at: 2/10/2015 4:22:10 PM |
|
12/22/2015 9:53 PM | |
Posts: 5225 Rating: (1189)
|
Thank you very much for letting us know! |
1/25/2018 10:25 PM | |
Posts: 1 Rating: (0) |
hi i have just installed tia v13 update 6 which update comes nextsome help please |
Follow us on