2/2/2018 5:37 PM | |
Posts: 1 Rating: (0) |
Hi, Don't mean to hijack this post but we're looking into a similar application where we would like to use a newer generation computer motherboard to run our Thermwood (wood cutting software). We have an isoPROFIBUS PCI card onto a newer generation motherboard i5 vs P4, we installed the 6AU1390-0AA00-0AA0 / isoPROFIBUS card into the new computer and moved over the XP installation as well, windows loads but the isoPROFIBUS card has an error coming up in device manager (error 37). We tried re-installing the driver to no avail and were hoping for an update to the driver or help with this error. Also we were wondering if this type of application would work (technically yes but are there other implications we've overseen?).. You suggestions and replies are greatly appreciated.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/5/2018 11:25:42 AMNew subject after splitting |
|
Follow us on