2/9/2018 8:01 PM | |
Posts: 1 Rating: (0) |
Hi, I have a bimba T-bot and was trying to get some advice on how to do the motion between the two servo motors that are mounted on this. I'm using two G120 drives. the t-bot has 1 belt running through the entire system, It kinda of works like an etch and sketch. What would be the best way to program this to use it like a pick and place. Any advice is appreciated. Cheers |
2/10/2018 8:49 AM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating: (150) |
Long time ago, there was an application for S7-315T with this kind of manipulator. You can check to see the forward and inverse kinematic models. You may translate in S7-1500T. https://support.industry.siemens.com/cs/ww/en/view/24094737 |
This contribution was helpful to1 thankful Users |
Follow us on