2/13/2018 2:15 PM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (83) |
Hi Nitin It is in the same computer. Do you have your database with WinCC? Because if you have it, then you don´t need internet connection to work with Database. If you have more information ... Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
Follow us on