6/25/2014 1:16 PM | |
Joined: 9/23/2005 Last visit: 10/4/2024 Posts: 4349 Rating: (1446)
|
Hi, the STEP7 Professional V13 Manual have information about Program_alarm (http://support.automation.siemens.com/WW/view/en/89515142) has information about how to configure Program_alarm at chapters 9.5.9 and 9.5.10. E.g. Alarm text are defined outside of the ladder, in the PLC Alarms "directory" (at project tree). in the text definicion, with right mouse click you can add "additional values" (tags, keywords and text lists). |
Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |
9/2/2014 10:52 PM | |
Joined: 7/7/2010 Last visit: 10/4/2024 Posts: 15264 Rating: (2422) |
There is also a Siemens created s7-1500/s7-1200 training kit with labs and slides configured. One of the labs walks you through creating custom alarm messages to appear in diagnostic buffer, on s7-1500 display, via web interface, and on hmi. If you can get Siemens to share with us the slides, or at least the part related to user alarms and post here, that would be fantastic for everyone. Maybe a FAQ :) |
science guy |
|
2/19/2018 10:12 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by a.giannotti is split to a separate thread with the subject How can display a real value?. Best regards |
Follow us on