2/16/2018 10:55 PM | |
Posts: 1 Rating: (0) |
I am having trouble migrating the tags and their properties in the tag spreadsheet generated by the export feature in Uticor PowerPanel v4 to the HMI tag table in WinCC Advanced V14 SP1. I don't understand the relationship between the HMI address given by PowerPanel and the address on the S7-300 PLC. I also don't know how to input that information into the tag table in WinCC. I've attached an excerpt from each spreadsheet to provide a reference. For example, in the PowerPanel format I believe that the address IW1/0 means that it is referencing the first bit of the first input word. How do I map that to the address on the PLC? How do I configure the corresponding entry in the WinCC tag table so that it accesses only that one bit instead of the whole input word? AttachmentSiemens Forum HMI Conversion Help.xlsx (24 Downloads) |
Follow us on