2/25/2018 9:33 PM | |
Posts: 5 Rating: (0) |
Hi! I created a button in WinCC and I just want to add a tag to this button. So i want a connection between WinCC and Simatic Manager. My goal when I click on the button the bit M0.0 should goes high. But when i want to choose this M0.0bit for tag it does not happen anything.. (the row stays orange) I made the WinCC project with the Wizzard, so the project is integrated in the Simatic Project. Here are some screenshots, please check it and help me! Thanks a lot! Attachmentscreenshots.zip (125 Downloads) |
2/25/2018 9:40 PM | |
Joined: 1/21/2013 Last visit: 10/23/2024 Posts: 4620 Rating: (708) |
Hello, Please have a look this FAQ it should be' like creating a button: https://support.industry.siemens.com/cs/ww/en/view/18660846 https://support.industry.siemens.com/tf/WW/en/posts/create-a-push-button/139354?page=0&pageSize=10 |
Last edited by: Ste39 at: 2/25/2018 9:49:40 PMLast edited by: Jen_Moderator at: 2/26/2018 12:32:41 PMOptimized link. |
|
This contribution was helpful to1 thankful Users |
Follow us on