3/13/2018 1:48 PM | |
Joined: 10/18/2012 Last visit: 10/21/2024 Posts: 225 Rating: (23) |
If you need profibus communication, then your PC requires a special communication port for profibus. Normal PC's usually don't have that interface and do only provide an Ethernet (RJ45) interface. For that you need an additional communication processor (CP), i.e. CP 5711, see for example Despite of the interface - I would recommend to use an Industrial PC (IPC), if you want to use it in an industrial production environment. You may have a look at the Panel-PCs overview webpage in the Siemens Mall: There you can find IPCs for Visualization (so called Panel-PC), which are developed for industrial use. If you are looking for a Siemens contact for more specific questions, then you can find one next to you at the following page: regards |
Follow us on