3/14/2018 7:57 AM | |
Posts: 17 Rating: (0) |
Hello on there, I want to monitor my project but when i click monitor the notificatoin go to STOP directly. this is the image of it --deleted Link-- although in my other programs isn't like this. My way to download my program is the same one and the others. My way to download program is be below this post, i just select my project and then click the icon of download. Anybody have suggestion for my problem, Thanks and Best Regards, RIZKY123 Attachmentpictures.zip (23 Downloads) |
Last edited by: RIZKY123 at: 3/14/2018 7:57:38 AMLast edited by: RIZKY123 at: 3/14/2018 7:58:39 AMLast edited by: Jen_Moderator at: 3/14/2018 2:37:01 PMDeleted link and added all files as an attachment. |
|
Follow us on