3/21/2018 4:46 PM | |
Joined: 8/5/2017 Last visit: 9/12/2022 Posts: 38 Rating: (1) |
I found in the PRODUCT INFORMATION that Qmax = 17 700 kg/h for DN 25 size, wich is the same default value for the upper scaling mentioned in the Operating Instructions manual (4.9 kg/s) (see image in attachment) but what makes me confused is that the maximum range is 24.5 kg/s ( 88200 kg/H). |
Follow us on