Industry Online Support
Technical Forum
8/11/2008 2:35 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi, -> look to this FAQ --> http://support.automation.siemens.com/WW/view/en/26187049 .... Project languages: A project in WinCC flexible can be created in up to 32 standard Windows languages. The requirement is that that your language choice has been loaded in the regional options in Windows. They can be found in the Control Panel under "Start > ("Settings") > Control Panel > Regional and Language Options (or "Regional Options")". There you can set the required options for the languages in which you wish to configure. Select the project languages in the following menu in WinCC flexible. (Fig. 02). Texts and text lists can then be edited in the selected languages..... so you have to check your Windows system if the language UK installed. When you create the project in english US and you change it to language UK then all "text-objects" must be translate again! |
8/11/2008 3:29 PM | |
Joined: 8/8/2008 Last visit: 4/24/2024 Posts: 78 Rating: (4) |
Yes, I thought that would be the case. No quick fix then hey? |
Follow us on