4/28/2018 11:40 AM | |
Posts: 4 Rating: (0) |
Hello folks, im designing some updates to our machinery but im bit stumped..i want to use the ET200ECO PN modules with ET200SP plc. I have never used et200 eco pn and im just wondering do i need to get some kinda master module for it on my ET200SP rack? Or can i just get those et200eco pn modules like this one 6ES7141-6BF00-0AB0 and just add them in hw config and off i go, or do i need the master like this 6ES7148-6JD00-0AB0 ..? |
4/28/2018 8:54 PM | |
Joined: 5/6/2010 Last visit: 6/2/2024 Posts: 1966 Rating: (274) |
Hello, of course you can start with the DI-modul. In my opinion is the best way to configure your system Hope this is helpful. regards |
Follow us on