5/12/2018 9:35 PM | |
Joined: 11/12/2017 Last visit: 2/27/2024 Posts: 174 Rating: (1) |
Hello again, Thanks for your help everyone. I have attached a few images on the next few posts of my setup to try and help you guys see what my problem is. I have the cable shown in the attached image connected to a USB port to my programming computer which is piggy-backed onto the HMI's profibus connector. This cable does work as I use it to download my programs from the same computer to my PLC's processor. The only thing I can think is wrong is that if you look at image called 'HMI Transfer settings' you will see it says MPI. Should this say DP? I only have the option of selecting MPI on the HMI. Although the station address and transmission speed is still correct. *My WinCC Flex project is integrated with my Step7 project if that makes any difference? Really appreciate the help! Thanks David AttachmentScreenshots.zip (389 Downloads) |
Last edited by: DS_7 at: 5/12/2018 9:40:04 PMLast edited by: Jen_Moderator at: 5/14/2018 8:10:51 AMAdded all pictures as an ZIP file. |
|
5/15/2018 11:06 AM | |
Joined: 11/12/2017 Last visit: 2/27/2024 Posts: 174 Rating: (1) |
Thanks for all your help Duris, greatly appreciate it! |
Follow us on