Industry Online Support
Technical Forum
8/20/2008 6:10 PM | |
Posts: 13 Rating: (0) |
How can I simulate WinLC RTX with plcsim? I Want test the system, plc and Winccflexible RT, on my computer. Thank you. Onire |
8/21/2008 1:18 PM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating: (1166) |
Dear onire77, Have you seen this link: http://support.automation.siemens.com/WW/view/en/16753950 And this one: it's about Protool, but it should also work with WinCC flexible: http://support.automation.siemens.com/WW/view/en/13283804 Best regards, Wizard |
8/21/2008 3:14 PM | |
Posts: 13 Rating: (0) |
Thanks Wizard, but it seems not work, as you can see in the picture.
Regards Onire |
8/22/2008 11:35 AM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (308) |
Hello, I was able to do the following: In my project I defined - one PC with WinLC RTX connected to profibus - one HMI station connected to Profibus using S7oline as interface. I have put the PG/PC interface on PLCSIM Profibus I started PLCSIM and I was able to dowload a small program I was able to create a small screen in WINCC Flexible and running the runtime displaying a clock memory. eveything was running in a single machine. See file in attachment for my settings This is may be enough for you to test. AttachmentPLCSIM+WINLC-RTX.pdf (317 Downloads) |
Best regards |
|
Follow us on