5/28/2018 7:13 AM | |
Joined: 5/15/2015 Last visit: 5/27/2024 Posts: 14 Rating: (0) |
Dear all! 2 machine has the same configuration and I have to put FM450 counter card (450-1AP00-0AE0) into s7 412-2XG04-0AB0 PLC. I downloaded the HW config and the blocks to the 1st machine well, but when I tried to download to the 2nd, I get an error message. The PG tried the download operation, but soon I get an error message: "The System data can't be loaded to module..." (I attached a short video) I checked the diagnostic wher I find this message: Event 1 of 120: Event ID 16# 530D How can I handle this issue? When I get this, I couldn't start the PLC. I removed the batteries to set the last config from memory card, because the PG couldn't connect to the PLC. Very strange that the 2 PLC is the same, I have not problem with the first, but i have problem with the second. Many thanks if someone can help me. AttachmentNEW PG Doesnt load to t23 bench 2018-05-26_13h47_28.avi (786 Downloads) |
Follow us on