5/29/2018 10:09 PM | |
Joined: 5/24/2018 Last visit: 2/7/2023 Posts: 26 Rating: (0) |
hello good afternoon, I tell you that I am commissioning a profibus network with abb acs800 drives, I already have the idea of what is a control word, reference, status word and current value I have to integrate the DCS system 8000xa of abb also, the Conuslta is that I'm using the proficore tool to commission the bus and I see my slave online but I want to write it so it works so I can see its input variables, I hope you can help me thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 5/30/2018 12:39:21 PMNew subject after splitting |
|
5/29/2018 11:04 PM | |
Joined: 9/27/2006 Last visit: 9/26/2024 Posts: 12283 Rating: (2685) |
Hello Hernan; Are you asking us (on a Siemens forum) how to setup Profibus comms for an ABB 800xa DCS system? If this is the case, maybe you should look into ABB documentation directly... https://new.abb.com/control-systems/system-800xa/800xa-dcs/fieldbus-protocols/profibus If I have understood your question incorrectly, please rephrase it more clearly. Hope this helps, Daniel Chartier |
5/30/2018 9:34 PM | |
Joined: 9/27/2006 Last visit: 9/26/2024 Posts: 12283 Rating: (2685) |
Hello Hernan; The only reference for Proficore that I can find on the web is a USB-interface for a Profibus analyser from Procentec:It is used as an interface between a Profibus network and either Profitrace or Proficaptain, analysers from Procentec. Profitrasce is a Profibus analyser tht can be used to debug a network: ProfiTrace 2.9.2 User Manual - Procentec ProfiCaptain is a external DP-master that can be used for commissioning the network: ProfiCaptain brochureAlone the Proficore USB interface is not very useful. Do you have any other Procentec harware/software in your installation? Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 5/30/2018 9:34:52 PM |
|
Follow us on