6/19/2013 4:04 PM | |
Joined: 3/4/2013 Last visit: 4/17/2023 Posts: 16 Rating: (0) |
First of All I want to thank you all for this thread. I am new to WinCC flexible. I had a situation in which customer wanted to log the User loging. I used the script method, and it worked perfectly. But there is one problem, When a User enter the wrong password by mistake and re-enter the correct password, the script wont log the last user login. I used I/O field to see the username (internet tag) , and its fine there. That means scheduler is working fine. Does anyone have any suggestion?
|
Last edited by: O_Moderator at: 6/20/2013 1:26 PMnew subject after splitting from /tf/WW/en/Posts/60569#top |
|
6/20/2013 3:31 PM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147)
|
Hello, Yes, when you change the user (username) the logging will be good. (Because the trigger is the change of user) Perhaps you can use the script in the following link: Why can you no longer log on to the operator panel (or WinCC flexible Runtime)? After logoff, the username is deleted. Now you will have to delete the username, when logon is not correct, by using wrong password. Best regards, Wizard |
6/21/2013 4:09 PM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147)
|
Hello, Can you post the scripts you are using now? Best regards, Wizard |
6/7/2018 10:30 AM | |
Joined: 6/19/2017 Last visit: 4/26/2024 Posts: 7952 Rating: (162) |
New question published by AmolK is split to a separate thread with the subject WinCC 7.4 Audit trail - actions are logging every time I operate it , but not showing old value and new value. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on