6/19/2018 3:40 PM | |
Joined: 6/30/2014 Last visit: 7/29/2024 Posts: 460 Rating:
|
Dear COMOS-Users and Admins, in case your SQL-list is empty, in COMOS 10.2.3 and you have entered the SQL-Entries into the registry by hand, I have a solution for you. Do not do the entries into the Windows registry by hand, but use the ODBC application (with the comfortable user interface) from Windows. That will enter the SQL list into the right path of the Windows registry, so you do not get into this issue. I saw that also in the official documentation of COMOS 10.2.3, attached here I hope this helps you a bit, please feel invited to enter here your experiences and feedback. Ciao SuperPippo AttachmentCOMOS 10.2.3 ODBC.pdf (216 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on