8/29/2008 8:27 PM | |
Joined: 12/20/2005 Last visit: 7/12/2023 Posts: 79 Rating:
|
lamgar, 1. The size and storage duration on CAS is based on the amount of data and the amount of disk space available. Below is alink to an FAQ that shows how much disk space is required on CAS based on number of archived tags, frequency and storage duration. As a rule of thumb, I would normally not exceed 60% ofahard disk'scapacity. After this period, the data could be moved to something like a DVD, where it could be restored whenever needed.
|
Follow us on