7/11/2018 7:03 AM | |
Joined: 10/24/2016 Last visit: 5/16/2024 Posts: 6 Rating: (0) |
hello my friends i have big problem in my system i have a system with two server and five client that one of server is standby .my servers use RAID hard . i use pcs7 7.1 sp3 in my system . suddenly on of server destroy that hang up i installed all of the software on it and downloaded my project . after restart system when system start up the problem repeat system wait on STATION CONFIGURATION EDITOR on 5% and hang up when i see the windows task manager there is many server running !!!! i attached picture do you have any idea? ------------------------------------------------------------------------------------------ |
Last edited by: kemitrio at: 7/11/2018 7:03:47 AMLast edited by: kemitrio at: 7/11/2018 11:19:55 AMLast edited by: kemitrio at: 7/11/2018 11:21:35 AMLast edited by: Jen_Moderator at: 7/11/2018 1:53:21 PMNew subject after splitting |
|
7/11/2018 1:54 PM | |
Joined: 6/19/2017 Last visit: 5/31/2024 Posts: 8110 Rating: (165) |
Closed cause question posted twice.
|
My Forum is the place to personalize your profile, |
|
Follow us on