7/12/2018 6:15 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873) |
Yes it can be 840D SL. It works with 611D. Please refer SINUMERIK 840D sl/840Di sl/840D/840Di/810D, SIMODRIVE 611digital, SINAMICS manual.
Hello, Yes this can happen. Since there is problem in power cable, when vertical axis is enabled, the axis servo loop is put into operation & motor is supposed to hold axis in position. But because power was not delivered to motor, (becuase of cable problem,) axis didnot hold at position & axis droped down due to gravitaional force. But I surprised, why the drive or controller did not pop up alarm / fault of motor overcurrent, or drive fault or motor stanstill position etc.etc. Please check NC data & PLC logic once again. HTH. |
Follow us on