7/17/2018 3:06 PM | |
Posts: 1283 Rating: (105) |
Can you delete and re-add the connection to see what are the option you have in connections? Thanks, Jay |
7/17/2018 3:24 PM | |
Posts: 70 Rating: (0) |
I remove and re add the connexion, but nothing has changed in the window of connexions. can you see the second attached image, i see that the HM_RT_1 is no connected ??? Attachmentimg.zip (96 Downloads) |
7/17/2018 3:38 PM | |
Posts: 70 Rating: (0) |
Yeah, its about PG/PC interface, Thanks so much Jay and Wizard |
This contribution was helpful to1 thankful Users |
7/17/2018 3:47 PM | |
Posts: 1283 Rating: (105) |
yes. That should be the first thing i asked him to check. Jay
|
Follow us on