6/28/2018 8:40 AM | |
Posts: 9 Rating:
|
Hi, I tried using the method attached below to connect m SIMATIC IOT2000 to my Windows computer. However, whenever i tried connecting the Putty.exe to my SIMATIC IOT2000, it will just appear that i have a Network error: Connection timed out and shows that it is inactive. The ip address of my computer/wifi is 172.30.27.143 and my ip address for the SIMATIC IOT2000 is 172.30.27.145 .
AttachmentSIMATIC_IOT2000_Setting_up_V2.0.pdf (356 Downloads) |
7/6/2018 7:07 AM | |
Posts: 9 Rating:
|
Hi, my computer is connect to the internet through the WIFI and my SIMATIC IOT is connected to my computer through the LAN cable at port 2. |
Follow us on