7/20/2018 5:23 AM | |
Posts: 9 Rating:
|
Hi i would just like to ask if it is possible to connect a 5v sensor to my SIMATIC IOT 2040 and how should i wire it up. |
7/20/2018 2:35 PM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating:
|
Hi, as I see you can use the sensor with or without the shield you mention in your post. The sensor can be provided with 5-24 Volts. If you are using 5 volts you can't use the shield; if you are using 24V you will have to use it. Supposing you will use 5V without the shield you can use the example Arduino sketch for example. Maybe you have to adapt the interrupt pin to 2 or 3. I am not sure if the DQs of the IOT2000 are fast enough to read in the PWM signal of the sensor. This has to be tested. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on