7/27/2018 1:19 PM | |
Joined: 8/3/2009 Last visit: 5/17/2024 Posts: 12970 Rating: (1651)
|
Hello Rockon in WinCC Comfort Advanced you cannot define the dynamisation like this! In WinCCProfessonal RT it would be easy, here you can select with a script first the correct index and set then the Times to the Properties of the Trend listing which you need. -> But in WinCC Comfort/Advnaced the Control isn´t as mighty as in Professional. so you cannot dynamise this. Use here not the Property list, use the Property pages for all possible dynamisations! If you need more help for using the F(x) Control in Comfort/Advanced you can use this one: https://support.industry.siemens.com/cs/ww/en/view/109481693 Bye Murof |
Last edited by: Murof at: 7/27/2018 1:20:54 PMIf this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on