8/7/2018 6:07 AM | |
Joined: 5/21/2018 Last visit: 7/12/2021 Posts: 49 Rating: (1) |
Step Number assignment in Graph Hello experts, I would like to assign a step number to a variable in the Graph program. For example, during the flow of the (Automatic) program, if an emergency stop is pressed, I would like to assign the current step at which the program at present to a variable, and exit out of the program to do a (Homing) home positioning, and once returning, I would like to start from the same position (Step) at which I exited the program (Automatic). I know to use in other languages like SCL. But not yet used in Graph. Can any one give a tip how to do it. Here with I attach you a snap shot oft he Graph for a view. If possible with snap shots. Hope to hear from you. Thank you. With regards AttachmentStepNumberAssignment.pdf (28 Downloads) |
8/7/2018 11:57 AM | |
Joined: 5/21/2018 Last visit: 7/12/2021 Posts: 49 Rating: (1) |
Hello Expert, Thank you for your response. I went through the manual and tried to do something, but did not get to the point. I have attached you a pdf file. Can you have a look at it and give an idea how to handle it. I mainly wanted to do it in Automatic mode. But currently I have tried to do it through Manual mode to test it. Hope to hear your feed back. Thank you. AttachmentStepAssignment.pdf (26 Downloads) |
Follow us on