7/28/2018 10:47 AM | |
Posts: 1 Rating:
|
Hello all, I have issue while using UDT which i have made. I have project with S7-400 CPU, and i have made UDT for motor,and then i made new DB , and make tags like Motor1, Motor2.. with data type motor. but when i want to use that tags in FC , like motor1.RunFB in logic, its not showing me, or showing me undefined Tag. please any one can suggest me for the same. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/30/2018 11:47:49 AMNew subject after splitting |
|
8/7/2018 1:32 PM | |
Joined: 3/27/2012 Last visit: 6/9/2023 Posts: 32 Rating:
|
Don't forget to put DB name in front. It should look like "Motors".Motor1.RunFB. |
Follow us on