8/16/2018 2:45 PM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Please also see attached screenshots. I have made a small function comparing the value of an integer with 4 different integers and writing a (different) integet to a DB value. In the new FC I have used a Word input and an Integer output and 5 bolean temporary variables. What will happen when I download the new FC and the modified FB to the PLC? Will the PLC go into stop or error? If that happens can it just be restarted and move on with the values and setpoints intact? Will I loose operator typed_in setpoints and similar and what can be done to avoid this? AttachmentFC1210.zip (72 Downloads) |
Follow us on