8/21/2018 2:48 PM | |
Joined: 3/14/2008 Last visit: 5/31/2024 Posts: 2070 Rating: (928)
|
Hi Boost34, If you set bit 6 to "1", then the block operates as continuous integrator. The Out.Value is set according to formula: "Out.Value = Out.Value n-1 + SampleTime/TI * (In.Value + In.Value n-1)/2". But you are using the block (with bit6=0 and bit7=1) as continuous summer. The Out.Value is set according to formula: "Out.Value = Out.Value(n-1) + Incr.Value" So, yes use Incr.Value instead of In.Value |
Last edited by: Oreca at: 8/21/2018 2:49:16 PMLast edited by: Oreca at: 8/21/2018 2:51:03 PMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on