8/25/2018 1:39 AM | |
Joined: 4/5/2016 Last visit: 2/19/2024 Posts: 1 Rating: (0) |
I am using TIA 14 SP1. Just started a new project with S7 1500F-2PN. V2.50 Since TIA 14 is not compatible with Firmware v2.5 Can I downgrade the firmware to v2.1. I am duplicating a previous project which had the same CPU but v2.1. firmware. Is there any danger in downgrading this firmware? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/27/2018 11:01:49 AMNew subject after splitting |
|
8/25/2018 2:19 AM | |
Joined: 3/28/2015 Last visit: 11/7/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topic might help: New Firmware Version V2.5 for SIMATIC S7-1500 and ET 200 CPUs Compatibility between CPU firmware and display firmware: Configuration of a CPU with Firmware V2.5 in TIA Portal Versions < V15: New properties of the CPUs with Firmware 2.5: |
Last edited by: Jen_Moderator at: 8/27/2018 11:31:46 AMOptimized link. Last edited by: Jen_Moderator at: 8/27/2018 11:37:53 AMOptimized missing links. Eng.Mohamed Ibrahim |
|
This contribution was helpful to3 thankful Users |
Follow us on