8/28/2018 6:54 AM | |
Joined: 8/3/2017 Last visit: 6/11/2024 Posts: 1086 Rating: (53) |
Hi AutoGen, I wouldn't recommend to buy this via ebay. You can use the trial version: https://support.industry.siemens.com/cs/at/en/view/109747981 And to learn it fast there are a lot of topics in the forum, which might be useful for you: At the end I think you have to buy the license Best regards, Noodles |
Please, check out the forum search to find already existing topics regarding your issue and to get some hints. |
|
8/29/2018 11:58 PM | |
Joined: 9/27/2006 Last visit: 11/12/2024 Posts: 12293 Rating: (2691)
|
Hello; To add some information to the very good suggestions already proposed, the order number you used for your thread title is for Step 7 v5.5 SP4. Unless the Siemens rep youcontact has a copy in his desk, the only trial license available now is for Step 7 v5.6. It is an adaptation of Step 7 v5.5 to Win10, but it also works with 64-bit versions of Windows 7. Here is a download link for Step 7 v5.6: Where do you procure the current trial software for STEP 7 V5.6? https://support.industry.siemens.com/cs/ww/en/view/109747981 Once you have your software (and PLCSim if possible, or some available CPU to test your programs on), I can suggest you look at these tutorials prepared by Siemens for automation students. Use the "Classic" modules for Step 7 v5.6. They present an increasing complexity of programming utilities from the very basic to more advanced modules as you go along, and we can help you out if something makes you struggle along the way. Training tutorials from Siemens: https://w3.siemens.com/mcms/sce/en/advanced_training/training_material/pages/default.aspx Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on