5/24/2010 1:52 PM | |
Joined: 2/10/2010 Last visit: 7/5/2024 Posts: 22 Rating:
|
Hi guys, Inmy recent projectI want to connect Siemens Sentron PAC3200 devices to the WinCC V7.0 SP1 via Modbus TCP. Using standard Modbus TCP driver in WinCCI established communication andI'm are able to read from PAC (from holding register, function code 0x04). Unfortunately I'm not able write to the registers (function code 0x06). For example I want to reset energy counters. Based on the information from PAC3200 manual (fig 3.) I defined tag EM_reset as shown on the fig.1.When I want to write to the tag nothing happens and also I have tag status - address error (fig.2.). Obviously something is wrong with addressing but I'm not sure exactly what. Also I didn’t found any explanation about file parameter in address properties, fig.1. Please can you give some advice how to solve this issue? P.S. I’m using PAC3200 device with latest firmware version (V2.1.0). Kind regards Alen Attachmentfigures.zip (652 Downloads) |
9/6/2010 9:10 PM | |
Joined: 2/18/2010 Last visit: 6/19/2024 Posts: 3 Rating:
|
Hi https://support.industry.siemens.com/tf/ww/en/posts/34734/
|
Last edited by: CS Moderator at: 6/3/2015 9:26:58 AMcorrected link after migration to the new pages |
|
Follow us on