9/4/2018 8:28 AM | |
Joined: 11/15/2009 Last visit: 8/16/2024 Posts: 380 Rating: (47) |
Hello Sebastian, SICLOCK TC 400 does not send a valid time on plant bus. Please check SICLOCK TC 400 setup. Regards |
9/4/2018 2:49 PM | |
Joined: 10/12/2016 Last visit: 10/2/2024 Posts: 20 Rating: (1) |
Hello JOTST, Attached configuration of the SICLOCK TC400, I can not find the problem. Any suggestions? Thank you.
Attachmentconfiguration SICLOCK TC 400 09-04-18.txt (143 Downloads) |
9/5/2018 8:41 PM | |
Joined: 10/12/2016 Last visit: 10/2/2024 Posts: 20 Rating: (1) |
Hello JOTST Yes, that manual I read almost completely, and there are many things that do not close me, even that chapter you refer to. I attach a document with the configuration I tried. Something that I lacked to clarify, according to the manual, we recommend "PCS 7-compatible mode, every 10 seconds", and I only have the options: "S7 compatible mode ..." or "S5 compatible mode ..." or "off". I will wait to see if it fails again and notice by this means. Anyway, I'm still receiving suggestions.
AttachmentModif SICLOCK TC 400.docx (141 Downloads) |
Last edited by: Sebastian P at: 9/5/2018 8:50:36 PM |
|
Follow us on