5/7/2013 1:12 PM | |
Posts: 1530 Rating: (59)
|
Hello FINS, QuickHeal Antivirus Scanner it not free for WinCC. Please take a look at your WinCC Information System and look there for "Antivirus", than you will get information, as I don't know which version of WinCC you are working with. You also can use compatibility tool and select your WinCC Version and Further Products/Virus Scanner With what are SIMATIC WinCC V7.x, V 6.x and V5.x compatible? If you want to have a quick view you also may use compatibility lists at end of this FAQ. Best regards Bizur Best regards Bizur |
9/7/2018 9:43 AM | |
Joined: 10/30/2007 Last visit: 6/11/2024 Posts: 7 Rating: (1) |
I have the same problem and tried the above suggestions. I have attached a link to the project, should anyone want to try. The project was sometime V6, but migrated to V7. I migrated it to V7.4. The MigratorLog shows no errors on the CS database. It is not possible to add any TagLogging: cannot add a single tag, or a new ProcessValueArchive. I was able to change the computername in the WinCC project, so the database seems to be writeable. (Don't know if the TagLogging is configured in the same database, or in the runtime database). [snip] For your information: I was able to make it working by taking the Original V6 project and first reorganizing it. Then converting it to V7.0 and V7.4 gave me a working project! AttachmentMP_Kranen_SVI_20180907(mig-schoon).zip (676 Downloads) |
Last edited by: Jen_Moderator at: 9/7/2018 11:43:32 AMRemoved link and added file as an attachment. Last edited by: Ton at: 9/13/2018 8:26:04 AM |
|
This contribution was helpful to1 thankful Users |
Follow us on