Industry Online Support
Technical Forum
9/3/2008 9:55 AM | |
Joined: 6/12/2008 Last visit: 7/4/2024 Posts: 18 Rating:
|
Can any body tell us, What is the diffrence between "SED2 Variable Speed Driveand Micro Master". Regads Shahzad Rehman |
9/3/2008 10:50 AM | |
Joined: 9/27/2006 Last visit: 8/6/2024 Posts: 12273 Rating:
|
Hello Shahzad; The SED2 line of VFDs are optimized for HVAC applications (for variable-torque pumps and fans, and for low harmonics generation). They are designed to work with SBT (Siemens Building technologies) Desigo HVAC controllers, andsupport communication interfaces to LON and Metasys. Here is a descriptive brochure on the SED2 VFDs that will give you more information: http://www.buildingtechnologies.siemens.com/NR/rdonlyres/78097848-8931-481F-B42A-CDE8705BB3C4/0/ZB00580401EN.pdf TheMicromaster line of VFDsare part of the A&D unit od Siemens, can be configured forconstant-torque or variable-torque applications, can implement simpleV/f control or more complex vector control in low-voltage industrial applications. They also communicate through USS protocol or Profibus-DP. Hope this helps, Daniel Chartier |
9/6/2008 1:48 PM | |
Posts: 148 Rating:
|
Good one Mr.Daniel Chartier |
9/9/2008 8:30 AM | |
Joined: 6/12/2008 Last visit: 7/4/2024 Posts: 18 Rating:
|
Thanks alot Regards Shahzad Rehman |
Follow us on