1/3/2013 7:55 PM | |
Posts: 4 Rating: (0) |
Hi, can someone tell how it is possible to upload the software from an HMI (KPT600) with TIA Portal Basic V11 SP2? Thanks |
3/6/2013 7:02 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Use Prosave in order to take a backup of HMI project. (not editable after). http://support.automation.siemens.com/WW/view/en/28928853 Best regards, Hristo Mihalev
|
3/6/2013 1:16 PM | |
Posts: 90 Rating: (0) |
Hi. Right, but there is no way to upload the complete "WinCC Flex" project in manner that I can edit it? Regards, Denker
|
3/6/2013 2:00 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Unfortunately, yes there is no way. Best regards, Hristo Mihalev
|
This contribution was helpful to1 thankful Users |
3/7/2013 6:46 AM | |
Joined: 8/31/2010 Last visit: 5/20/2024 Posts: 1512 Rating: (223) |
Hello Denker, You can still do it. There is one way of doing it which is called "Back Transfer". Have a look atthis - How do you back transfer the projects of an operator panel and what should you watch out for? Hope this helps. But still this functionality is missing in TIA Portal v11 also in the latest v12.atleast hope this comes in the upcoming SPx |
Like it? Rate it! |
|
This contribution was helpful to2 thankful Users |
9/17/2018 1:25 PM | |
Posts: 1 Rating: (0) |
Please tell me where is the option to upload backup from hmi |
Follow us on