9/21/2018 11:26 PM | |
Posts: 24 Rating: (0) |
Hello all, I would like to setup an IRT communication, but I'm not allowed to tick the box in the picture, why? What do I need to do? Beginner23 |
9/22/2018 8:24 AM | |
Posts: 24 Rating: (0) |
Hello again, Thanks for the answer. I include a project with the setup. I would like to communicate with IRT to the node and the DI IO. But I can not tick the box and I get an error when I compile. Thanks Beginner23 AttachmentIRT.zip (153 Downloads) |
9/22/2018 5:30 PM | |
Posts: 24 Rating: (0) |
Thanks! But it support IRT? What is the different between IRT and isochronous mode? |
9/23/2018 7:44 AM | |
Joined: 5/12/2006 Last visit: 9/2/2024 Posts: 22348 Rating: (3006) |
Hello, this means that you can use this device in IRT Networks because the Chipset can work with IRT Frames but the device itself can not work isochronous. https://support.industry.siemens.com/cs/ww/en/view/44383954 Regards Christoph |
Follow us on