9/26/2018 10:43 PM | |
Posts: 11 Rating:
|
Dear Friends I'm going to implement a time stamping application with ET200M (6ES7 153-2BA01-0XB0) and CPU313C-2DP . According to catalog of ET200M, it's necessary for DP master to support DPV1 to be able of time stamping. So, I'm wondering if DP port of CPU313C-2DP supports DPV1 or not. I've read following instructions: How can you tell whether your S7-300/400 master supports DPV1 ... Product Information Conversion to DPV1 FAQ ... - Siemens Support The first link proposed a procedure to detect which s7300 CPUs supports DPV1. I've installed the GSD V5 for IM153-2 (6ES7 153-2BA01-0XB0), unlike what is said in this procedure, after installation of GSD, still it's not possible to change between DPV0 and DPV1 in DP operating mode off CPU. The second link, stated "In the S7-300 family, the CPUs with MMC support the DPV1 master functionality as of firmware version 2.0" I'm confused which one is correct?! As you can see in attachment, in the property dialog of CPU315C-2DP (DP-Operating Mode tab) there is no option for selecting DPV1, while for S7-400 CPUs it can be selected. finally, can i use DP port of CPU313C-2DP for DPV1 functionality. Please give me your suggestion. Sincerely ------------------------------------------------------------------------------------------ AttachmentDPV1.pdf (128 Downloads) |
Last edited by: NaAhoora at: 9/26/2018 10:43:54 PMLast edited by: The Helping Hand at: 9/27/2018 9:39:40 AMNew subject after splitting |
|
9/27/2018 11:51 AM | |
Posts: 11 Rating:
|
Dear Christoph/mop Thank you . I've tested several CPUs like (6ES7 313-6CF03-0AB0-V2.6) and (6ES7 317-2AJ10-0AB0-V2.6). As you can see in attachment (DPV1-IM153.pdf), I've installed the gsd. But the DPV0/DPV1 you've mentioned is not displayed in parameter setting of ET200M. Sincerely AttachmentDPV1-IM153.pdf (130 Downloads) |
Follow us on