10/2/2018 2:58 PM | |
Joined: 9/27/2006 Last visit: 4/27/2024 Posts: 12257 Rating: (2665) |
Hello KRN; Possibly you might find the information in the following FAQ interesting: https://support.industry.siemens.com/cs/ww/en/view/109482719 As you can see in the screenshot below, WITH sTEP 7 V5.3 AND HIGHER, you can use the GSD file for Profibus or Profinet to integrate the 6ES7 531-7PF-0AB0 as part of an ET 200MP station, with an interface module IM 155-5 DP ST V3.0 (Order no.: 6ES7 155-5BA00-0BA0). You can only insert it as part of the Hardware Configuration of a S7-1500 in TIA Portal. Hope this helps, Daniel Chartier |
Follow us on