Industry Online Support
Technical Forum
4/9/2008 2:07 PM | |
Posts: 1776 Rating: (95)
|
Hi, look at this FAQ http://support.automation.siemens.com/WW/view/en/5668269 |
4/23/2008 3:29 AM | |
Joined: 1/21/2008 Last visit: 7/12/2024 Posts: 39 Rating: (14) |
Miffo, If I grabbed the correct file from my archive then this should contain a sample. Check for the code that adjust the time-zone, there are actually WinCC script functions that give you the local time, so the script can be simplified. It runs in PCS 7 V7.0 SP1, earlier versions may work as well Ronald Nijssen AttachmentAlarmDetailPdl.zip (248 Downloads) |
9/11/2008 3:22 PM | |
Posts: 6 Rating: (0) |
GMsgFunction |
Follow us on