9/10/2018 8:45 PM | |
Joined: 2/8/2018 Last visit: 2/5/2024 Posts: 8 Rating: (0) |
I have a similar problem just with a new Simotion, when turning it on or connecting it to the power supply the LEDs STOPU, STOP, BUS1F and BUS2F oscillate near 20 Hz, I tried to reset the memory as the manual says but they remain the same and In addition to pinging the factory IP of the Simotion Ethernet port I have no answer, I tried with crossover cable, with normal utp cable, using a switch as an intermediary and even then I have no response from the port of Simotion and also by MPI I can not connect. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/11/2018 9:27:05 AMNew subject after splitting |
|
10/8/2018 9:08 PM | |
Joined: 2/8/2018 Last visit: 2/5/2024 Posts: 8 Rating: (0) |
Thanks, but I don't have the 2nd DVD, that's why I was asking where I can find how to do the update. |
Follow us on