8/2/2016 1:56 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating:
|
Hello aleb2, I know how to do this in WinCC Professional. It doesn't wirk directly witch Advanced, because you need C-scripting. With a little effort you might still be able to adapt if for WinCC Advanced. It would work like this: You have an executable C-script (.exe, .batch?) which is taking a specified window and puts it in the foreground. The script is started by using the system function "StartProgram". You can find the code to put a window in front in the following FAQs.
Alternatively don't hide the task bar or run the WinCC Advanced runtime in window mode. |
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to
1 thankful Users |
Follow us on